RLS

Electric motors

RLS is strongly rooted in drive technology and has been developing advanced sensor solutions for speed and position detection (commutation) for various electric drives for decades.

"The variety on the market is huge, we needed the best technology that would fit into our motors. RLS were happy to adapt and tailor their existing magnetic encoder products to our needs." TQ-RoboDrive (Germany)

Many drive manufacturers trust our OnAxis encoders, as well as bearingless encoders like RoLin, AksIM and Orbis. They are all based on highest quality, robustness and sustainable technologies. We are also happy to accept individual challenges and realize modifications and special solutions.

How do encoders in electric motors work?

Brushless motor


Challenge:

Built-in rotary encoders are used to indicate the angle of the motor shaft in brushless permanent magnet motors. In such cases, the encoder serves as a feedback device, which is crucial for the proper operation of the equipment. Brushless motors require electronic commutation, often partly achieved by using rotor magnets as low resolution absolute encoders (typically six or twelve pulses per revolution). The resulting shaft angle information is transmitted to the servo drive so that it can excite the correct stator winding at any time.

Solution:

For the BLDC motor to function properly, the controller (drive) must know the position of the rotor. To achieve this, zeroing should be carried out. Zeroing is a process in which an alignment of the electrical and mechanical position is achieved. In this way the controller knows through which winding a current should be sent.

SPEED

Speed detection can be achieved with incremental encoders, from compact encoders such as RMBs, RMs, to bearingless encoders such as RoLin or AksIM, as well as redundant and space-saving solutions. We are also happy to implement modifications and special solutions.

POSITIONING

A servomotor is a closed-loop servo mechanism that uses position feedback to control its movement and end position. For this application, absolute encoders like AksIM or Orbis are mainly used. The input to its control is a signal (either analog or digital) representing the commanded position for the output shaft. The motor is paired with a type of encoder to provide position and speed feedback. The measured position of the output is compared with the commanded position, the external input to its control. If the output position deviates from the target position, an error signal is generated which then causes the motor to rotate in both directions to bring the output shaft to the corresponding position. As the positions approach, the error signal is reduced to zero and the motor stops.

Why RLS magnetic encoders?

Industry Challenges

  • Reliability
  • Repeatability
  • Low weight and compact size
  • Low energy consumption

RLS Solutions

  • Good price-performance ratio
  • Wide range of available sizes
  • Wide range of resolutions
  • Industry standard absolute or incremental output options
  • High dynamic response
  • High accuracy
  • Large installation tolerances
  • High reliability
  • Non-contact 360° rotation or linear position detection
  • Low power consumption
  • Immune to stray external magnetic fields

Recommended products

New
FlexAB™

FlexAB™

Absolute Magnetic Scale System for Large Diameters

New
AksIM-4™ HIPERFACE DSL®

AksIM-4™ HIPERFACE DSL®

Off-axis Rotary Absolute Magnetic Encoder

Upcoming
Orbis™ Housed

Orbis™ Housed

Through-hole Rotary Encoder

AksIM-4™ Big Rings

AksIM-4™ Big Rings

Off-Axis Rotary Absolute Magnetic Encoder

New
FlexIN™

FlexIN™

Magnetic Scale System for Large Diameters

New
Orbis™

Orbis™

Rotary Magnetic Encoder Module

AksIM-2™

AksIM-2™

Off-Axis Rotary Absolute Magnetic Encoder Module

LA12

LA12

Absolute Magnetic Encoder System with Mitsubishi, Yaskawa and Fanuc Serial Communication

HiLin™

HiLin™

High-accuracy Linear Magnetic Encoder System

RM08

RM08

Miniature Rotary Magnetic Encoder

AksIM-2™ Redundant

AksIM-2™ Redundant

Off-Axis Rotary Absolute Magnetic Encoder Module

LinACE™

LinACE™

InAxis Linear Absolute Magnetic Shaft Encoder

LA11

LA11

Linear Absolute Magnetic Encoder

RMB14

RMB14

Rotary Magnetic Encoder Module

RMB20

RMB20

Rotary Magnetic Encoder Module

RMB20 with AM4096 chip

RMB20 with AM4096 chip

Rotary Magnetic Encoder Module with AM4096 chip

RMB23

RMB23

Rotary Magnetic Encoder Module

RMB28 / RMF44 / RMF58 with AM4096 chip

RMB28 / RMF44 / RMF58 with AM4096 chip

Rotary Magnetic Encoder Module with AM4096 chip

New
RMB28 / RMF44 / RMF58

RMB28 / RMF44 / RMF58

Rotary Magnetic Encoder Module

RMB28 with SATI03

RMB28 with SATI03

Rotary Magnetic Encoder Module

RMB29

RMB29

Rotary Magnetic Encoder Module

RMB30

RMB30

Rotary Magnetic Encoder Module

RLB

RLB

Miniature Incremental Magnetic Encoder Module

RLC2IC

RLC2IC

Miniature Incremental Magnetic Encoder Module

RLC2HD

RLC2HD

Miniature Incremental Magnetic Encoder Module

RLM

RLM

Miniature Incremental Magnetic Encoder

AksIM™ Housed

AksIM™ Housed

Off-Axis Rotary Absolute Magnetic Encoder