成功案例
了解我们的客户如何使用RLS编码器解决实际工程挑战。
-
Printing · Automation
Redefining Repeatability in Screen Printing with the Artos Encoder System
INO integrates the Artos absolute linear encoder system into its PRINT M family of screen printing machines to achieve precise table positioning and eliminate time-consuming homing sequences.
-
Robotics
Enabling High-Precision Hollow Shaft Actuation with AksIM-2 Encoders
MAB Robotics integrated RLS AksIM-2 encoders into compact hollow-shaft actuators to achieve precise, reliable position feedback without compromising actuator size or performance. -
Subsea robotics
The Miniature RM08 Encoder: Supporting Autonomous Underwater Systems
Teledyne Gavia achieved precise and reliable AUV flap control in harsh subsea conditions using the compact RM08 rotary encoder.
-
Electric motors
Efficiency in Electric Propulsion with RM44 Encoders
Asruk improves efficiency and reliability of high-performance electric motors using RM44 magnetic encoders from RLS.
-
Automotive
绝对式编码器赋能 Spanesi 新一代汽车维修机械臂
Spanesi partnered with RLS to redesign its Touch measuring system by replacing optical encoders with AksIM absolute magnetic encoders.
-
Electric motors
Magnetic Encoders in High‐torque Motors for Reliable Performance
Alva Industries uses RLS AksIM encoders in its SlimTorq™ motors to deliver compact, high-torque performance with precise, reliable feedback.
-
Robotics
OnAxis Encoders Enable Graspian’s Advanced Robotic Grip
RMB20 helps Graspian bring human-like dexterity to robotic gripping by providing precise, real-time motion feedback that enables adaptive, touch-sensitive control of each finger.
-
Robotics
AksIM-2系列编码器在四足机器人领域的应用
AIDIN ROBOTICS enhanced their quadruped robot's dynamic balance and precise motion control by integrating compact, reliable AksIM-2 encoders from RLS into each joint.
-
Robotics
AksIM™ supports French collaborative robot in industrial automation
MS-Innov's MORFOSE cobot integrates AksIM-2 encoders for high precision, adaptability, and efficiency.
-
Electric motors
How ThinGap uses RLS magnetic encoders for precise motion control
AksIM‐2™ provides precise motion feedback for high‐performance motors.
-
3D printing
How encoders enable consistent quality in additive manufacturing
The LA11 readhead with the SAS10 magnetic scale enhances Meltio’s 3D printer accuracy and reliability.
-
AGV
Compact and precise: RLS encoders powering MiR AMRs
RoLin and OnAxis encoders provide precise position feedback in AMRs while optimizing system compactness.
-
Exoskeleton · Robotics
Pioneering pediatric exoskeletons with high-precision encoders
RE:HOME uses AksIM-2 encoders to enhance exoskeletons for children with cerebral palsy, enabling natural movement.
-
Robotics
RLS编码器显著提升Sparkfield健身器材的效率和安全性
Sparkfield enhances its robotic fitness device with AksIM-2 encoders, ensuring precise, safe, and adaptive strength training.
-
Electric motors · Drives
Enhancing building performance: Magnetic encoders in active mass dampers
CALMFLOOR采用RLS编码器,无需对建筑结构进行改动即可有效缓解楼层振动,从而提升改造空间的建筑性能与可持续性。
-
Electric motors · Drives
RLS为Wavedrive解决方案提供具有优异性价比的磁编码器
Wavedrive解决方案集成RLS编码器,为定制精密驱动系统及医疗设备提供高性能且具成本效益的位置反馈。
-
Electric motors · Drives
RLS磁编码器如何革新电机行业
Zero Motorcycles通过集成RLS传感器,优化电机控制性能并延长续航里程,显著提升电动汽车的可靠性与能效。
-
Medical
RLS磁编码器帮助提高仿生假肢使用者的生活质量
Revival Bionics通过采用RLS编码器,显著改善足部假肢的性能,使膝下截肢人士能够实现平稳、自然的行走步态。
-
Medical
RLS编码器助力上海联影医疗打造世界级医疗器械
UIH在其CT扫描仪中采用RLS编码器,实现高速、精确成像,全面提升诊断能力。
-
Virtual reality · Simulators · Automotive
RLS磁编码器和雷尼绍助力Dynisma登顶领先地位
Dynisma uses RLS encoders to achieve low-latency motion simulation, providing realistic driver feedback essential for automotive and motorsport applications.
-
Virtual reality · Simulators · Aerospace
RLS Sensors – a Crucial Part of a VR Simulator and Aerobatic Aircraft Hybrid
AFormX employs RLS encoders in its hybrid aerobatic flight simulators, offering advanced pilot training with precise control feedback.
-
Robotics · Exoskeleton
Project MARCH全力为脊髓损伤患者打造先进外骨骼机器人
RLS encoders ensure precise joint control in Project MARCH's exoskeletons, aiding individuals with spinal cord injuries in mobility and independence.
-
Robotics · Exoskeleton
RLS磁编码器助力Marsi Bionics打造“改变生活”的外骨骼机器人
Marsi Bionics的外骨骼机器人搭载RLS编码器,为行动不便的儿童和成人提供精确、灵活的运动支持。
-
Electric motors · Drives
磁编码器战胜尺寸和速度挑战
RLS encoders in microrobots provide the accuracy and speed necessary for competing in and winning autonomous maze-solving contests.
-
Electric motors · Drives
雷尼绍与RLS联手推动机器人变革
TQ-RoboDrive integrates RLS encoders in its ultra-light, high-torque motors for compact, efficient robotic applications.
-
Laboratory
RLS编码器在3DHISTECH显微镜内部发挥关键作用
3DHISTECH将RLS编码器集成于数字切片扫描仪中,以提高大型病理学实验室的切片处理效率和扫描精度。
-
Robotics · Exoskeleton
PAL Robotics借助磁编码器技术实现机器人运动平衡
RLS encoders help PAL Robotics achieve balance and precision in humanoid robots, enhancing their functionality in dynamic environments.
-
Laboratory
磁编码器助力制造性能可靠的晶圆传送机器人
RLS编码器是RND晶圆传送机器人的重要组成部分,可确保半导体制造过程的高精度与高可靠性。
-
Virtual reality · Simulators
虚拟现实 - RLS和雷尼绍编码器的精度和重复性助力实现完美的视频技术。
Power Plus employs RLS encoders for precise camera positioning in VR setups, enhancing live virtual broadcasts with seamless integration.
没有符合此过滤条件的结果。
我们支持学生STEM项目
We support students in their educational STEM projects, that aim to discover and awaken the next generation of engineers.
了解更多