성공 사례

저희는 글로벌 시장 요구에 부응하기 위해 첨단 로터리 및 리니어 모션 센서를 설계, 생산 및 공급합니다.

The Miniature RM08 Encoder: Supporting Autonomous Underwater Systems

The Miniature RM08 Encoder: Supporting Autonomous Underwater Systems

Subsea robotics

Teledyne Gavia achieved precise and reliable AUV flap control in harsh subsea conditions using the compact RM08 rotary encoder.

Efficiency in Electric Propulsion with RM44 Encoders

Efficiency in Electric Propulsion with RM44 Encoders

전기 모터

Asruk improves efficiency and reliability of high-performance electric motors using RM44 magnetic encoders from RLS.

Compact and precise: RLS encoders powering MiR AMRs

Compact and precise: RLS encoders powering MiR AMRs

AGV

RoLin and OnAxis encoders provide precise position feedback in AMRs while optimizing system compactness.

Absolute Encoders at the Heart of Spanesi’s Next-Gen Repair Arm

Absolute Encoders at the Heart of Spanesi’s Next-Gen Repair Arm

Automotive

Spanesi partnered with RLS to redesign its Touch measuring system by replacing optical encoders with AksIM absolute magnetic encoders.

Magnetic Encoders in High‐torque Motors for Reliable Performance

Magnetic Encoders in High‐torque Motors for Reliable Performance

전기 모터

Alva Industries uses RLS AksIM encoders in its SlimTorq™ motors to deliver compact, high-torque performance with precise, reliable feedback.

OnAxis Encoders Enable Graspian’s Advanced Robotic Grip

OnAxis Encoders Enable Graspian’s Advanced Robotic Grip

로봇공학

RMB20 helps Graspian bring human-like dexterity to robotic gripping by providing precise, real-time motion feedback that enables adaptive, touch-sensitive control of each finger.

Application of AksIM‐2 series encoders in quadruped robots

사족 로봇에 AksIM‐2 시리즈 엔코더 적용

로봇공학

AIDIN ROBOTICS enhanced their quadruped robot's dynamic balance and precise motion control by integrating compact, reliable AksIM-2  encoders from RLS into each joint.

How encoders enable consistent quality in additive manufacturing

How encoders enable consistent quality in additive manufacturing

3D printing

The LA11 readhead with the SAS10 magnetic scale enhances Meltio’s 3D printer accuracy and reliability.

AksIM™ supports French collaborative robot in industrial automation

AksIM™ supports French collaborative robot in industrial automation

로봇공학

MS-Innov's MORFOSE cobot integrates AksIM-2 encoders for high precision, adaptability, and efficiency. 

How ThinGap uses RLS magnetic encoders for precise motion control

How ThinGap uses RLS magnetic encoders for precise motion control

전기 모터

AksIM‐2™ provides precise motion feedback for high‐performance motors.

Project MARCH races to build advanced exoskeleton for people with a spinal cord injury

척추 손상 환자를 위한 첨단 외골격 개발에 박차를 가하고 있는 Project MARCH

로봇공학, Exoskeleton

RLS encoders ensure precise joint control in Project MARCH's exoskeletons, aiding individuals with spinal cord injuries in mobility and independence​.

Transforming Lives with RLS Magnetic Encoders in Bionic Prostheses

바이오닉 보철에 RLS 마그네틱 엔코더를 사용했을 때의 삶의 변화

의료

RLS encoders enhance the performance of Revival Bionics' foot prostheses, enabling smooth, natural movement for below-knee amputees.

Pioneering pediatric exoskeletons with high-precision encoders

Pioneering pediatric exoskeletons with high-precision encoders

Exoskeleton, Robotics

RE:HOME uses AksIM-2 encoders to enhance exoskeletons for children with cerebral palsy, enabling natural movement.

Enhancing building performance: Magnetic encoders in active mass dampers

Enhancing building performance: Magnetic encoders in active mass dampers

전기 모터, Drives

CALMFLOOR uses RLS encoders to mitigate floor vibrations without structural alterations, enhancing building performance and sustainability in repurposed spaces.

RLS encoders maximize the efficiency and safety of Sparkfield fitness device

RLS 엔코더, Sparkfield 피트니스 기구의 효율성과 안전성 극대화

로봇공학

Sparkfield가 정밀하고 안전한 적응형 근력 운동이 가능하도록 AksIM-2 엔코더로 로봇 피트니스 기구를 개선하고 있습니다.

RLS provides the best price-performance magnetic encoders for Wavedrive solutions

RLS, Wavedrive 솔루션을 위한 최고 가성비의 마그네틱 엔코더 제공

전기 모터, Drives

RLS encoders in Wavedrive solutions provide cost-effective, high-performance position feedback for custom precision drives and medical devices.

Shanghai United Imaging Healthcare uses RLS encoders to build world-class medical equipment

Shanghai United Imaging Healthcare, RLS 엔코더를 사용하여 세계적인 수준의 의료 장비 개발

의료

UIH leverages RLS encoders in its CT scanners to achieve high-speed, precise imaging, enhancing diagnostic capabilities globally.

How RLS Magnetic Encoders are Revolutionising the Electric Motor Industry

RLS 마그네틱 엔코더가 전기 모터 산업계에 혁신을 가져오는 방식

전기 모터, Drives

Zero Motorcycles integrates RLS sensors to optimize motor control and extend range, improving the reliability and efficiency of their electric vehicles.

RLS encoders and Renishaw help place Dynisma in pole position

RLS 엔코더와 Renishaw, Dynisma가 유리한 위치를 선점할 수 있도록 지원

Virtual reality, Simulators, Automotive

Dynisma uses RLS encoders to achieve low-latency motion simulation, providing realistic driver feedback essential for automotive and motorsport applications​.

RLS Sensors – a Crucial Part of a VR Simulator and Aerobatic Aircraft Hybrid

RLS Sensors – a Crucial Part of a VR Simulator and Aerobatic Aircraft Hybrid

Virtual reality, Simulators, Aerospace

AFormX employs RLS encoders in its hybrid aerobatic flight simulators, offering advanced pilot training with precise control feedback​.

PAL Robotics integrates magnetic encoder technology into robots to achieve balance

PAL Robotics, 마그네틱 엔코더 기술 통합으로 로봇 균형 유지

로봇공학, Exoskeleton

RLS encoders help PAL Robotics achieve balance and precision in humanoid robots, enhancing their functionality in dynamic environments.

Renishaw and RLS help to drive a robot revolution

Renishaw와 RLS, 로봇 분야의 혁신 주도

전기 모터, Drives

TQ-RoboDrive integrates RLS encoders in its ultra-light, high-torque motors for compact, efficient robotic applications​.

Magnetic encoders contribute to reliable wafer transfer robots

웨이퍼 이송 로봇의 신뢰성을 높여주는 마그네틱 엔코더

Laboratory

RLS encoders are integral to RND's wafer transfer robots, ensuring precision and reliability in semiconductor manufacturing processes.

Virtual Reality – The beauty of vision technology with the accuracy and repeatability of RLS and Renishaw encoders.

가상현실 ??? 정확하고 반복 가능한 RLS 및 Renishaw 엔코더를 통한 아름다운 시각 기술

Virtual reality, Simulators

Power Plus employs RLS encoders for precise camera positioning in VR setups, enhancing live virtual broadcasts with seamless integration​.

Magnetic encoders beat size and speed challenges

마그네틱 엔코더로 크기와 속도 문제 해결

전기 모터, Drives

RLS encoders in microrobots provide the accuracy and speed necessary for competing in and winning autonomous maze-solving contests​.

RLS magnetic encoders enable Marsi Bionics to build life-changing exoskeletons

Marsi Bionics는 RLS 마그네틱 엔코더를 통해 인생을 바꿔 주는 착용형 외골격 로봇이 되었습니다

로봇공학, Exoskeleton

Marsi Bionics uses RLS encoders in exoskeletons to provide accurate, dynamic movement support for children and adults with mobility impairments.

RLS encoders go under the 3DHISTECH microscope

3DHISTECH 현미경에 RLS 엔코더 사용

Laboratory

3DHISTECH integrates RLS encoders in its digital slide scanners to increase throughput and accuracy in large pathology labs.

학생 STEM 프로젝트 지원사

RLS 엔코더는 설치가 쉽고 매우 다양한 방식으로 사용할 수 있기 때문에 학생과 관련된 광범위한 분야에서 활용되고 있습니다. RLS는 차세대 엔지니어를 발굴하고 육성하는 것을 목표로 하는 교육 STEM(Science(과학), Technology(기술), Engineering(엔지니어링), Maths(수학)) 프로젝트를 통해 학생들을 후원합니다.

자세히