RLS

Max Encoder Resolution Calculator

As an illustration, consider an encoder with an operating frequency of 150 kHz and a maximum shaft speed of 1,200 RPM.

The max encoder resolution can be computed using the following formula:

Max Encoder Resolution = Operating Frequency (kHz) × 60,000 / Max RPM

Plugging in the values:

150 kHz × 60,000 / 1,200 RPM = 7,500 PPR

This suggests that the encoder, under these conditions, would support a maximum resolution of approximately 7,500 PPR.

Calculate Max Encoder Resolution