Linear and Ring Magnetic Technology
26 articles
No questions in this category match your search.
Also found in other categories
No questions match your search.
- What is the structure and thickness of magnetic scales?
- How to install magnetic scale?
- How to cut magnetic scales correctly?
- How do I know which scale length to choose and what is the minimum distance from edges of scale for positioning the reference mark?
- When is better to use stick-on reference than machined reference mark?
- What does minimum edge separation mean and which do I have to choose?
- What are the specifications of scale adhesive tape?
- How do the cover foil and stick-on reference mark affect the ride height?
- What happens if the stick-on reference mark is applied incorrectly?
- Why use the cover foil?
- How to order the cover foil?
- Can LM encoder systems be used in linear motors?
- What is the structure of magnetic ring?
- How long is the shelf life of magnetic scales and magnetic rings?
- How to install the magnetic ring?
- Is it possible to order just the ring without the readhead and is it possible to order custom size rings?
- Accuracy
- What is the MTTF (Mean Time To Failure) for linear and ring encoders?
- What magnetic fields will damage the magnetic scale?
- What is interpolation, cpr, and ppr?
- What is the maximum temperature the scale can withstand?
- Can linear / ring magnetic encoder systems be used in vacuum environments?
- How big is high-frequency noise of analogue signals?
- Can magnetic scale be bent and installed onto a circular surface?
- What is the duty cycle of A and B digital output signals?
- What is the requirement for the substrate flatness for scale installation?