RLS
Orbis

Is there an Incremental Orbis?

Yes.

Orbis for commutation (Ux output) provides both A, B, Z incremental signals and UVW commutation signals. If the UVW signals are not required, they can simply be left unconnected, while using only the A, B, and Z signals.

In both configurations, setting the zero position by pressing the two pads remains available.

お探しのものが見つかりませんか? 詳細については、お問い合わせください。