A message to our customers and suppliers about COVID-19. Learn more

返品

In addition to your right to cancel, you can return the standard products (interfaces, accessories, magnets and rings) bought on this website within 30 days from when you received the package if the products have not been used. A 10% restocking fee will be applied.

The configured products (encoders, scales) are customized just for you. That means we cannot accept returns, except for manufacturing defects.

不具合品の返品は常時受け付けています。

注: すべてのエンコーダとコンポーネントには、1 年保証が付随します。

返品時の送料はお客様負担でお願いいたします。返品に使用する業者について、特に制限はありません。

The products returned as a result of a defect caused on the side of RLS will be replaced or refunded in full. Please ensure you return these to us as soon as possible.

Please follow the instructions below for returns:

  1. Contact our Sales Support team (sales@rls.si) and fill out the GRA - Goods Return Authorisation form.
  2. 記入したフォームをスキャンして、sales@rls.si に E メールで送付します。
  3. セールスサポートチームが返信します。
  4. Package the products with a copy of the invoice and GRA form and send them to the address below:
"Reclamations"
RLS Merilna tehnika d. o. o.
Poslovna cona Zeje pri Komendi
Pod vrbami 2
SI-1218 Komenda
Slovenia
お探しのものが見つかりませんか? 詳細については、お問い合わせください。