How is the cable length measured?
The cable length is measured from the rim of the encoder body to the end of the flying leads or the connector.
For flying leads
The length of the flying leads is always 35 mm of which 5 mm are completely stripped, tinned and ready for soldering.

For all connector types

Didn’t find what you were looking for?
Contact us for more info.