Studentenprojekte
Wir unterstützen Studenten während ihrer Ausbildung bei MINT (Mathematik, Informatik, Naturwissenschaft und Technik) Projekten.
Driving Dexterity: RLS Encoders Power Binghamton’s 6-Degree of Freedom Arm
Competing in the demanding University Rover Challenge, the Binghamton University Rover Team integrated RLS AksIM-2™ absolute magnetic encoders to provide the high-resolution feedback necessary f...
RLS Magnetic Encoders Enable Precise Navigation in Autonomous Robots
Hyperion Robotics student team achieved precise and reliable navigation in autonomous competition robots by using RLS RE36 absolute magnetic encoders.
Blue Flash Advancing Driverless Racing with RLS Sensors
Blue Flash uses RLS sensors to drive reliable, precise innovation in their driverless Formula Student race car.
Guided by Precision: Orbis Encoders at Propulse NTNU Rockets
Propulse NTNU uses RLS's Orbis™ encoders for precise valve control in rockets and drones, ensuring reliable performance in extreme conditions.
The advantages of the magnetic encoders in space rover technology
Xplore has developed a rover capable of traversing extraterrestrial landscapes, focusing on the role of magnetic encoders in its development and improvement.
Der Weg zum Sieg: RLS Messsysteme in den Rennwagen des Revolve Studierendenverbands der NTNU
Revolve NTNU utilizes RLS encoders in their electric racing cars, ensuring precision in control systems for competitive racing.
Das Racing-Team der University of Nottingham dankt RLS für seinen jüngsten Erfolg
The team uses RLS angular position sensors in pedal and steering assemblies, enhancing control in their high-performance racing vehicles.
Rays Wetterstation
RLS encoders are used in a weather station's wind vane to accurately measure wind direction, aiding in reliable meteorological data collection.
Wie magnetische Messsysteme zur Verbesserung der Genauigkeit eines SCARA eingesetzt werden
Austrian students enhanced the accuracy of a SCARA robot by integrating RLS magnetic encoders, improving its precision in automated tasks.
Clever Kameleon
A multi-purpose Martian rover developed by the Kameleon Team at Opole University, integrating RLS encoders for precise movement and task execution in a variety of environments.
Magnetische Messsysteme unterstützen die Stabilisierungskontrolle eines selbstbalancierenden Zweirad-Roboterfahrzeugs
RLS magnetic encoders provide precise stabilization and control for a self-balancing two-wheeled robotic vehicle, ensuring smooth and reliable operation.
ROBI – Ein Prototyp des mobilen Manipulators für landwirtschaftliche Anwendungen
ROBI’ is a prototype mobile manipulator for agricultural applications with requirements of low-cost, low-weight, simplicity, flexibility and modularity.
RLS Messsystem hilft beim Bau eines Formel-1-Rennwagens im Formula Student-Konstruktionswettbewerb
Team Tallinn is the first and only Estonian Formula Student team, founded in 2006, which consists of students from Tallinn University of Technology and Tallinn University of Applied Sciences.