Sine/Cosine
Sinusoidal outputs produce one period of sine and cosine signal per turn (360°).
Analogue sinusoidal outputs
Complementary Sine/Cosine
The outputs are differential sinusoids in quadrature.
Analogue differential sinusoidal outputs
Unbuffered/Buffered outputs from the ASIC
Unbuffered output means that the signals generated by the rotation of the shaft are transferred directly from the sensor output. Unbuffered outputs have a typical output impedance of 10 kΩ.
Buffered output means that the device incorporates a built-in amplifier with an output impedance of 720 Ω.