How to order the cover foil?

There are two options:

1. You can order the magnetic scale with the cover foil
2. You can order the cover foil separately

When ordering the magnetic scale which includes the cover foil the length of the cover foil is always provided 5 cm longer than the scale. This additional length can be used to protect the ends of the scale and secure to the substrate.

Similarly, when ordering the cover foil separately we suggest that the cover foil is at least 5 cm longer than the length of the scale for the same reasons.

Didn’t find what you were looking for? Contact us for more info.