Is CE certificate available for AksIM encoders?
CE is not available, because:
- We can’t provide radio frequency interference (RFI) compliance for the product without housing.
- An encoder is not a plug-and-play device. MBA readheads don’t even have a cable.
- Whenever user modifies the electrical circuit or mechanical assembly (adding a cable, cover, mounting to the surface, etc.) original CE certification would become invalid and user must make certification for the complete product.
There are other certificates available for Conflicting minerals, RoHS, etc. They are available in the FAQ - COMMERCIAL section of the website.