What is the structure and thickness of magnetic scales?

The magnetic scale is structured as shown in the image below.

 

Magnetic scale structure

 

 

 Magnetic scale thickness
  With back adhesion Without back adhesion
No cover foil, cut or magnetised reference mark 1.5 ±0.15 1.3 ±0.15
No cover foil, stick-on reference mark 1.5 ±0.15 1.3 ±0.15
With cover foil, cut or magnetised reference mark 1.6 ±0.15 1.4 ±0.15
With cover foil, stick-on reference mark 1.6 ±0.15 1.4 ±0.15
Didn’t find what you were looking for? Contact us for more info.