MTTF calculator
The Mean Time To Failure (MTTF) for RM/RE encoders can be calculated using the formula:
M = p× t / n
Where:
- M is the Mean Time To Failure value.
- t is average length of service.
- n is the total relevant failures.
- p is the installed population of readheads.
To provide a hands-on example, consider a scenario where an encoder readhead has a Mean Time To Failure (MTTF) of 500 years, which suggests non-stop usage. If there is a customer who owns 30 machines, and each machine is fitted with 4 encoders, then the aggregate number of installed readheads (p) comes to 120. To determine the average duration (t) between any single readhead breakdown (i.e., n = 1), the MTTF formula can be restructured as:
t = M × n / p = 500 years× 1/120 = roughly 4,17 years
So, with an overall count of 120 readheads operating all day, every day, the customer can anticipate a single readhead malfunction around every 4.17 years.
This information is not a guarantee of product reliability and does not represent a condition of warranty.
Calculate average length of service:
Calculate All encoder calculators