如何選擇編碼器

輸出、讀取類型和編碼器機身的選擇繁多,該如何找出最適合自己應用方式的理想感測器?

How to choose between Nonius and AksIM technology

For Nonius technology, the magnetic code carrier consists of two magnetic encoder tracks. The outer track consists of an even number of alternately magnetized poles and is used for high-precision position determination. It is therefore referred to as the master track. The second inner track has one fewer pair of poles than the outer track and is therefore referred to as the Nonius track. This track is used to calculate an absolute position within one revolution of the pole disk. This is done by calculating the angular difference between the two tracks. Encoders with this technology must be calibrated before use. An alternative option to Nonius technology that does not require calibration is AksIM technology.

如何選擇適用於 RLS 編碼器的正確軟體和介面?

RLS has developed a few software for use with RLS encoders.