学生项目

We support students in their educational STEM (Science, Technology, Engineering and Maths) projects.

The Road to Victory: RLS Encoders in Revolve Racing Cars

The Road to Victory: RLS Encoders in Revolve Racing Cars

Revolve NTNU is a student organisation at the Norwegian University of Science and Technology (NTNU), Trondheim campus. Since 2010, they have evolved from racing cars with internal combustion engines to four-wheel drive electric racing cars that can be driven manually or autonomously.

Magnetic encoders support the stabilisation control of a self-balancing two-wheeled robotic vehicle

RLS磁编码器增强两轮自平衡机器人小车的稳定性控制

University of Nottingham Racing Team thanks RLS for its recent success

诺丁汉大学赛车队感谢RLS助其取得最近一场胜利

RLS supply us with a range of angular position sensors which we use in our pedal and steering assemblies, and they have a wide selection of options available for various sizes, applications, and high-speed operations.

ROBI - A Prototype Mobile Manipulator for Agricultural Applications

ROBI — 适合农业应用的移动机械手原型机

ROBI’ is a prototype mobile manipulator for agricultural applications with requirements of low-cost, low-weight, simplicity, flexibility and modularity.

Rays Weather Station

Rays气象站

The wind vane is responsible for determining which direction the wind is coming from. Inside the wind vane rotating cap there is a radially oriented magnet attached to the center bolt which rotates with the wind vane. Its position is sensed by the RLS RMK2 hall effect angle sensor.  The se...

Using magnetic encoder to improve the accuracy of a SCARA

使用磁编码器提升SCARA的精度

It is quite common in Austria, that students of a final class of a school for higher technical education, must prove their knowledge by working on a final project. Thus, two students of the LiTec in Linz, Austria have decided to design a robotic arm. Due to the cooperation with RLS and their generou...

Clever Kameleon

Clever Kameleon

Clever Kameleon is a project carried out at the Opole University of Technology by the Kameleon Team. Since 2015 the goal is to build and develop a multi-purpose Martian rover. The main targets of the project are the development of its members, students of the Opole University of Technology and parti...

RLS encoder helps to build Formula Student formula car

RLS编码器助力打造大学生方程式赛车

Team Tallinn is the first and only Estonian Formula Student team, founded in 2006, which consists of students from Tallinn University of Technology and Tallinn University of Applied Sciences.

RLS编码器的成功案例

我们设计、生产并提供先进的旋转和直线运动传感器,以满足全球市场需求。

了解更多