如何选择编码器

要从各种输出形式、读取类型和编码器尺寸中做出选择,如何确保针对具体应用选出最佳的编码器?

How to choose between Nonius and AksIM technology

For Nonius technology, the magnetic code carrier consists of two magnetic encoder tracks. The outer track consists of an even number of alternately magnetized poles and is used for high-precision position determination. It is therefore referred to as the master track. The second inner track has one fewer pair of poles than the outer track and is therefore referred to as the Nonius track. This track is used to calculate an absolute position within one revolution of the pole disk. This is done by calculating the angular difference between the two tracks. Encoders with this technology must be calibrated before use. An alternative option to Nonius technology that does not require calibration is AksIM technology.

如何正确选择与RLS编码器配合使用的软件和接口?

RLS has developed a few software for use with RLS encoders.